Feedback_Iq_min

Index.Sub 2230.0FH
Data Type Unsigned16
Access Read/Write
PDO Mappable

No

Unit

milliamperes (mA)

Range

Unsigned16
Default Value

500

Store Supported Yes
Description

 This value is used for Closed Loop feature and defines minimum amplitude of the phase’s current. It can also be considered as minimum current applied at the motor.

Notes

--